Question
STM32L IWDG reload with different prescaler
Posted on August 06, 2014 at 23:31
Hi everyone,
In my project, i need to use iwdg. I use 2 iwdg init function. Prescaler is 256 and reload is 15seconds for the first one.Prescaler is 32 and reload is 1.45seconds for the second one.Both of them is working when I am using 32MHz cpu clock, however, the second one is not work when I use 4MHz cpu clock. What could be the possible mistake?Best regards