STM32L 32.7680Khz Clock Problem
Hello,
after several Years of using the 32L475RET6 with a 12pF 32.7680KHz Crystal and 8.2pF Capacitors we need to change the PCB to a 32L486QG. As to read in the Datasheet both have 5pF Pin Input Capacity.
But the new Design (Chrystal about 1.5mm away from IC ) wont start. The Crystal (changed several Times also against a 9pF ) wont start. When i put a Finger on the Capacitors he will start and the Device is running as long my Finger is on the PCB.
The STM32L4 is switching between run mode and sleep mode several Times in his Application.
Until now i have no Idea whats going on..
Any Idea ??
Thanks and Greetings
*****