Skip to main content
MJack.1
Associate III
April 28, 2021
Question

STM32H755 dual core debugging issue is related to BOOT_CM4 option byte

  • April 28, 2021
  • 1 reply
  • 893 views

Hi all,

I'm editing this post because the forum doesn't allow me to delete it, and it might help someone else..

I was having an issue where simply generating a default NUCLEO-H755ZI-Q project from the current latest CubeMX for Cube IDE and following the debugging instructions in the following application note exactly, did not work.

I tried lots of suggestions on various posts, but for me it turned out to be that the M4 BOOT option byte was disabled, which is why I couldn't debug the M4.

I resolved it with the STLink utility.

Cheers

This topic has been closed for replies.

1 reply

Technical Moderator
May 11, 2021

Thank you @Community member​  for updating your post to share the solution.

This will help other community members finding answers to their issues ;)

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks