Skip to main content
篠良光.1
Visitor II
February 10, 2021
Question

STM32H753�?�質�?�?��?�。クロック�?�20Mを使用�?30903Hz入力信�?��?�1周期を分解能�?�16ビット�?��?�100回�?AD変�?��?�測定�?��?��?��?�考�?��?��?��?��?�。�?��?�場�?��?�変�?�精度�?��?��?��?�?��?�ょ�?��?�?�?��?�マイコン内�?��?�種設定を教�?��?��??�?��?��?�。無�?��?�場�?��?�使用�?�能�?�マイコン�?�設定方法を教�?��?��??

  • February 10, 2021
  • 1 reply
  • 522 views

..

This topic has been closed for replies.

1 reply

Amel NASRI
Technical Moderator
February 12, 2021

Hi,

Welcome to the ST Community :)

You have more chance to get an answer if you used English to ask your question as it is the common language here.

I try to translate your question using an online tool:

This is a question for STM32H753. I want to use 20M clock and AD convert one cycle of 30903Hz input signal 100 times each with 16 bits of resolution and measure it. What is the conversion accuracy in this case? Also, please tell me the various settings in the microcomputer. If this is not possible, please tell me the microcomputers that can be used and the setting method.

I assume you want to configure ADC on STM32H753. I suggest that you start with STM32CubeMX to setup the configuration you need.

If you still need help, please try to precise your requirement here.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.