STM32H743 SDIO interface low voltage mode help improve speeds ?
Hello, I am designing massive board with STM32H743 and 10CL120YF780I7G FPGA, so I want best of the best for periferals.
It is good idea to have SDcard interface to load large data sets or save large tables to SDCard.
As far as i rememmber STM32F4 was not very fast with SDcards, but how about STM32H7 ? IT does say that supports 100MHz SDIO interface as well as low voltage mode where i need separate chip to work, but what is the gains of this modification ?
Does it allows to have higher speed ? Does it also helps to use larger cards, like 64GB like SanDisk Extreme PRO UHS1/3 ?
I was unable to find any data on this....