Skip to main content
rwareinc
Associate III
July 31, 2019
Solved

Stm32h7 Memory location for boot on the M7 core and the M4 core? Looking for a detailed explanation on boot or start up procedure for a dual core product.

  • July 31, 2019
  • 3 replies
  • 898 views

..

This topic has been closed for replies.
Best answer by Uwe Bonnes

What are you missing in RM0399?

3 replies

Uwe Bonnes
Uwe BonnesBest answer
Chief
July 31, 2019

What are you missing in RM0399?

rwareinc
rwareincAuthor
Associate III
July 31, 2019

Turns out RM0399 is what I was missing... had RM0433, this covers it. Thanks

Tesla DeLorean
Guru
August 15, 2019

Options define start addresses/modes

Notionally the dual-port flash is shared, lower half to M7 (0x08000000), upper half to M4 (0x08100000), and most the lower bandwidth peripherals living in the same domain as the M4, but accessible to both.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..