Skip to main content
shanmugam
Associate
April 26, 2016
Question

STM32F429NIH6 interfacing with Memory

  • April 26, 2016
  • 2 replies
  • 625 views
Posted on April 26, 2016 at 13:55

Hi,

I have interfaced two SDRAM and two NAND flash with STM32F429NIH6 Microcontroller. I have shared the 16-bit data bus with all of the devices mentioned above. All are operating with 3.3V supply, SDRAM CKE and CS# are individual signals for each device. Input capacitance for SDRAM is 6pf max and NAND flash is 10pf max. 

Is the Microcontroller can able to source without any malfunction or should we need to provide any bidirectional buffer in between Microcontroller and Memory devices?

Quick response is highly appreciable.

Thanks in advance.

Regards,

Shanmugam N
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    April 26, 2016
    Posted on April 26, 2016 at 15:14

    How much memory are you using that requires two of each memory?

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
    shanmugam
    shanmugamAuthor
    Associate
    April 27, 2016
    Posted on April 27, 2016 at 15:06

    Each SDRAM memory size is 64Mbyte(32M x 16) and each Flash memory size is 256Mbyte(128M x 16).