Skip to main content
ugniues
Associate
July 17, 2015
Question

STM32F411RE NUCLEO board doesn't work

  • July 17, 2015
  • 2 replies
  • 847 views
Posted on July 17, 2015 at 13:55

Good day,

I'm pretty new with stm32 microcontrollers and I have some trouble, so I would like to ask you for help. Yesterday I downloaded Visual Studio and VisualGDB for programming. Everything worked fine, I uploaded few times test application with blinking LED. After that I tried to test button. I didn't find any tutorials so I tried to write something by myself (Now, I think that was a stupid idea). I wrote something like this:

#include <
stm32f4xx_hal.h
>
#ifdef __cplusplus
extern ''C''
#endif
void SysTick_Handler(void)
{
HAL_IncTick();
HAL_SYSTICK_IRQHandler();
}
int main(void)
{
HAL_Init();
__GPIOA_CLK_ENABLE();//Clock for LED
__GPIOC_CLK_ENABLE();//Clock for Button
GPIO_InitTypeDef GPIO_InitStructure;
GPIO_InitStructure.Pin = GPIO_PIN_5;//LED pin
GPIO_InitStructure.Pin = GPIO_PIN_13;//Button pin
//Led 
GPIO_InitStructure.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStructure.Speed = GPIO_SPEED_HIGH;
GPIO_InitStructure.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStructure);
//Button
GPIO_InitStructure.Mode = GPIO_MODE_INPUT;
GPIO_InitStructure.Speed = GPIO_SPEED_HIGH;
GPIO_InitStructure.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOC, &GPIO_InitStructure);
for (;;)
{
if (HAL_GPIO_ReadPin(GPIOC, GPIO_PIN_13)){
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_SET); 
}
else{
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_RESET);
}
}
}

Microcontroller successfully uploaded program, but it didn't work like I expected. After this I tried to get back to LED blinking but I got this error: [img]http://i.imgur.com/RGTJPrk.png[/img] Did I killed STM32F411 or this is something fixable? Thank you. #error #nucleo
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    July 17, 2015
    Posted on July 17, 2015 at 14:22

    You need to program the pins individually, here you're breaking pin PA13 which is the debugger interface signal SWDIO

    Connect the BOOT[0] pin to VDD, connect to the board and erase the part with the ST-LINK Utilities, or equivalent applications.

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
    ugniues
    ugniuesAuthor
    Associate
    July 17, 2015
    Posted on July 17, 2015 at 14:42

    Thank you very much! It worked!