STM32F407G-DISC1 - cannot access memory
Hi,
after working with this board fine for a while I now have a problem. Using Keil when I tried to LOAD the program a message reads: 'Flash Timeout. Reset the Target and try again.'. I tried a lot of things, from simply removing it from the USB port and connecting again, to changing download options, which never worked.
I then proceeded to use ST-Link Utility to try and change the read/write protection. I cannot access the memory and that is what appears in the program 'Can not read memory. 'Disable Read out protection and retry.', which I cannot due because I cannot access its memory.
I am starting to think that the hardware may be somehow damaged, which if that is the case, I cannot figure out why.
Anyone got this problem and a solution?
#flash #stm32f4-discovery