Question
STM32F407 Timer Frequency
Posted on March 09, 2015 at 17:56
I can't understand how come TIM1 frequency is 42 MHz.
Here is my config: 12 MHz HSE -> 168 MHz PLLCLK (MCO/4 = 42 MHz, checked) APB1 prescaler = 4 APB2 prescaler = 2 so TIM1, as it clocked from APB2 x 2 frequency should be 168 MHz. But output (GPIO^PIN in update interrupt) generates 0.21 MHz frequency 0.21x100x2 = 42MHz. RCC_PCLK1Config(RCC_HCLK_Div4); RCC_PCLK2Config(RCC_HCLK_Div2); RCC_HCLKConfig(RCC_SYSCLK_Div1); TIM_TimeBaseStructure.TIM_Period = 99; TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure); #tim #stm32