Skip to main content
gavinli
Associate II
January 14, 2015
Question

STM32F407 captured value two times bigger than expected

  • January 14, 2015
  • 4 replies
  • 809 views
Posted on January 14, 2015 at 20:51

Hi, I have the MCU run SysClk at 168MHz, and I setup the timer to capture mode, but the returned value is two times bigger than expected. I checked the waveform of the toggled LED, it is correct, just the Timer capture value is bigger. Please help me understand why.

* Supported STM32F40xxx/41xxx devices 
*----------------------------------------------------------------------------- 
* System Clock source | PLL (HSE) 
*----------------------------------------------------------------------------- 
* SYSCLK(Hz) | 168000000 
*----------------------------------------------------------------------------- 
* HCLK(Hz) | 168000000 
*----------------------------------------------------------------------------- 
* AHB Prescaler | 1 
*----------------------------------------------------------------------------- 
* APB1 Prescaler | 4 
*----------------------------------------------------------------------------- 
* APB2 Prescaler | 2 
static uint16_t *buf_tim1; 
static uint16_t *buf_tim3; 
void capture_init(TIM_TypeDef* TIMx, uint32_t *buf, int total_samples_per_channel) 
{ 
/* TIM Update Frequency = TIM Clock / (P * Q) 
* 
* Where Prescaler = P - 1, and Period = Q - 1 
* 
* TIM1 input freq = 84MHz, it is in APB2 
* TIM3 input freq = 42MHz, it is in APB1 
*/ 
if ((TIMx != TIM1) && (TIMx != TIM3)) return; 
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; 
/* Time base configuration */ 
TIM_TimeBaseStructure.TIM_Period = ~0; // 65536us update // 0..FFFF 
if (TIMx == TIM1) 
TIM_TimeBaseStructure.TIM_Prescaler = 84 - 1; // 0..FFFF 
else 
TIM_TimeBaseStructure.TIM_Prescaler = 42 - 1; // 0..FFFF 
TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1; //TIM_CKD_DIV1, TIM_CKD_DIV2, TIM_CKD_DIV4 
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; 
TIM_TimeBaseInit(TIMx, &TIM_TimeBaseStructure); 
TIM_ICInitTypeDef TIM_ICInitStructure; 
TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising; 
TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI; 
TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1; 
TIM_ICInitStructure.TIM_ICFilter = 0x0; 
TIM_ICInitStructure.TIM_Channel = TIM_Channel_3; 
TIM_ICInit(TIMx, &TIM_ICInitStructure); 
TIM_ITConfig(TIMx, TIM_IT_CC3, ENABLE); 
TIM_ICInitStructure.TIM_Channel = TIM_Channel_4; 
TIM_ICInit(TIMx, &TIM_ICInitStructure); 
TIM_ITConfig(TIMx, TIM_IT_CC4, ENABLE); 
NVIC_InitTypeDef NVIC_InitStructure; 
if (TIMx == TIM1) { 
/* Enable the TIM1 global Interrupt */ 
NVIC_InitStructure.NVIC_IRQChannel = TIM1_CC_IRQn; 
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 4; 
buf_tim1 = (uint16_t*)buf; 
} 
else { 
/* Enable the TIM3 global Interrupt */ 
NVIC_InitStructure.NVIC_IRQChannel = TIM3_IRQn; 
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 5; 
buf_tim3 = (uint16_t*)buf; 
} 
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; 
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; 
NVIC_Init(&NVIC_InitStructure); 
/* TIM enable counter */ 
TIM_Cmd(TIMx, ENABLE); 
} 
void TIM1_CC_IRQHandler(void) 
{ 
static uint16 u00, u01, u10, u11; 
if (TIM_GetITStatus(TIM1, TIM_IT_CC3)) { 
u11 = TIM_GetCapture3(TIM1); 
TIM_ClearITPendingBit(TIM1, TIM_IT_CC3); 
buf_tim1[1] = u11 - u10; 
u10 = u11; 
gpio_toggle_pin(GPIOPortID_E, GPIOPinID_1); 
} 
if (TIM_GetITStatus(TIM1, TIM_IT_CC4)) { 
u01 = TIM_GetCapture4(TIM1); 
TIM_ClearITPendingBit(TIM1, TIM_IT_CC4); 
buf_tim1[0] = u01 - u00; 
u00 = u01; 
gpio_toggle_pin(GPIOPortID_E, GPIOPinID_0); 
} 
} 
void TIM3_IRQHandler(void) 
{ 
static uint16 u00, u01, u10, u11; 
if (TIM_GetITStatus(TIM3, TIM_IT_CC3)) { 
u11 = TIM_GetCapture3(TIM3); 
TIM_ClearITPendingBit(TIM3, TIM_IT_CC3); 
buf_tim3[1] = u11 - u10; 
u10 = u11; 
gpio_toggle_pin(GPIOPortID_E, GPIOPinID_3); 
} 
if (TIM_GetITStatus(TIM3, TIM_IT_CC4)) { 
u01 = TIM_GetCapture4(TIM3); 
TIM_ClearITPendingBit(TIM3, TIM_IT_CC4); 
buf_tim3[0] = u01 - u00; 
u00 = u01; 
gpio_toggle_pin(GPIOPortID_E, GPIOPinID_2); 
} 
} 
void main(void) 
{ 
uint16 capture[4]; 
//initializations 
..... 
capture_init(TIM3, (uint32_t *)&capture[0], 1); 
capture_init(TIM1, (uint32_t *)&capture[2], 1); 
while(1); 
} 

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    January 14, 2015
    Posted on January 14, 2015 at 22:05

    Please help me understand why.

    Review the Clock Tree diagram in the Reference Manual more carefully. The TIM CLK is typically 2* the APB clock in all but the DIV1 mode.
    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
    gavinli
    gavinliAuthor
    Associate II
    January 15, 2015
    Posted on January 15, 2015 at 18:02

    Hi, Clive1

    Thanks for your reply.

    I got another question. I have two kind of boards, one board (A) has TIM3_CH3 and TIM3_CH4 connected to MCU, and TIM1_CH3 and TIM1_CH4 floating. I only initialized TIM3 in my program, but there is not TIM3_CH3 interrupt, the TIM3_CH4 CC interrupt works fine.

    The other board (B) has all the TIM1, TIM3 CH3&CH4 connected, no matter I initialize one Timer or two Timers, they all work as expected.

    Trying to find out why board A not working, I set the TIM3 CH3 and CH4 pin to GPIO output mode, and I toggle thoese pins, the connection are all correct, because I saw the waves.

    So, It seems I did something wrong in the program. Would you please give me some idea? Thanks.
    Tesla DeLorean
    Guru
    January 15, 2015
    Posted on January 15, 2015 at 18:16

    Not sure I'm up for wading through all this.

    You're going to have to do some more coding for TIM1, the timebase and channel structures have more fields which need to be filled in.

    TIM1 (and TIM8) have a Repetition Count, N-Outputs, and the PWM Outputs (and Inputs) need enabling.

    If pin connectivity is a problem check the AF Pin Source configurations.
    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
    waclawek.jan
    Super User
    January 15, 2015
    Posted on January 15, 2015 at 22:22

    > TIM1 (and TIM8) [...] the PWM Outputs (and Inputs) need enabling.

    Ah, the TIMx_BDTR.MOE gotcha...

    It's maybe time to start the STM32 Frequently Encountered Gotchas list. Both the ''(F2/F4) timer runs twice as fast as expected'' and ''TIM1/TIM8 output won't work'' are in there...

    JW