Skip to main content
kruszi
Associate II
March 8, 2016
Question

STM32F4 Timer 2 / 5 using 32bit

  • March 8, 2016
  • 2 replies
  • 2020 views
Posted on March 08, 2016 at 15:15

Hi,

according to the reference manual the STM32F4(07) Timer 2 and Timer 5 are capable of counting 32bit. I want to use upcounting and overflow event. As far as I understand these timers, the timer counts from 0 to ARR (auto reload value), creates an overflow event and starts from 0 again.

Using STD Peripherals library you can see in stm32f4xx_tim.h

 

 

uint32_t TIM_Period;           

/*!< Specifies the period value to be loaded into the active                        Auto-Reload Register at the next update event. This parameter must be a number between 0x0000 and 0xFFFF.  */

Is loaded into ARR.

So my problem is, that I want to use 32bits of the timer and a ARR that is bigger than 16bit.

Any ideas why only 16bit auto reload values are allowed ?
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    March 8, 2016
    Posted on March 08, 2016 at 17:26

    Any ideas why only 16bit auto reload values are allowed ?

    The comment comes from the older F1 library, the value can be 0x00000000..0xFFFFFFFF

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
    Walid FTITI_O
    Visitor II
    March 9, 2016
    Posted on March 09, 2016 at 14:49

    Hi l..michael,

    That's depends on the device and which timer in that device you are using. Keep your first reference of information both reference manual and datasheet of that device.

    In your case , with STM32F407, it is mentioned in the reference manual, in TIM2 to TIM5 main features part page 582  the following: “16-bit (TIM3 and TIM4) or 32-bit (TIM2 and TIM5) up, down, up/down auto-reload counter.â€�

    For the driver/ headers are developed to support all kinds of integrated Timers and give the safe conditions to avoid inconvenience.

    So TIM2 and TIM5 contains 32-bit auto-reload counters and you can work with safely.

    -Hannibal-