Question
STM32F4 I2S Full Duplex: Is Double Transmit possible?
Posted on January 11, 2014 at 10:45
Hello,
I've been spending some time looking through the STM32F4 reference document and it looks quite clear that the I2S2 / I2S2ext are supposed to be used in a full-duplex configuration.However, I'm curious, is it possible to configure I2S2 as TX and I2S2ext as TX at the same time and use them independently ( transmit two different words at the same time )?Thanks,Phil. #stm32-i2s-duplex