Skip to main content
mkostek9
Visitor II
November 7, 2014
Question

STM32F4 Discovery ADC + DMA

  • November 7, 2014
  • 1 reply
  • 574 views
Posted on November 07, 2014 at 12:30

Hi there, I'm trying to use two ADC channels and send them to array via DMA.

Here is my code.

void
ADC_Config (
void
){
//Rozdzielczosc 12 bitow, 
//Wyrownanie bitow do prawej
ADC->CCR |= ADC_CCR_ADCPRE_0 | ADC_CCR_ADCPRE_1; 
//PCLK2/8=72MHz/8=9 MHz;
ADC1->CR1 = ADC_CR1_SCAN; 
//Scan mode Enable (do wykonania pomariu z kilku kanalow)
ADC1->CR2 = ADC_CR2_CONT; 
//Pomiar ciagly 
ADC1->SQR1|= ADC_SQR1_L_1; 
// wybor liczby pomiarow (2)
ADC1->SQR3 = ADC_SQR3_SQ1_1 | ADC_SQR3_SQ1_3; 
//Jako pierwszy pomiar wykonany jest na kanale 10 
ADC1->SQR3|= ADC_SQR3_SQ2_4; 
//Jako drugi pomiar - kanal 16 (termometr) 
/*The temperature sensor, VREFINT and the VBAT channel are available only on the master
ADC1 peripheral*/
//3 cykle dla kanalu 10
ADC1->SMPR1 |= ADC_SMPR1_SMP16_0 | ADC_SMPR1_SMP16_1 | ADC_SMPR1_SMP16_2; 
//480 cykli dla kanalu 16;
ADC1->CR2|= ADC_CR2_DMA; 
//Wlaczenie DMA
ADC->CCR |= ADC_CCR_TSVREFE; 
//Odpalenie termometru
ADC1->CR2 |= ADC_CR2_ADON; 
//Wlaczenie ADC1
//Kalibracja automatyczna
}
void
DMA_Config (
void
){
DMA2_Stream4->CR = 0; 
//Wylacz Stream4 dla DM2
while
(DMA2_Stream4->CR & DMA_SxCR_EN); 
//Czekaj tak dlugo, az bit EN=0. 
DMA2_Stream4->PAR = ADC1_DR_Address; 
//Adres docelowy 
DMA2_Stream4->M0AR = (unsigned 
int
)buforADC; 
//buforADC to tablica z wartosciami do przeslania 
DMA2_Stream4->NDTR=2; 
//Rozmiar przesylanej tablicy to 2
//ADC1 jest zglaszane na kanale 0
DMA2_Stream4->CR |= DMA_SxCR_PL_1; 
//Ustawienie priorytetu na wysoki
//Kierunek przesylania danych: pamiec -> peryferia 
DMA2_Stream4->CR |= DMA_SxCR_MINC; 
// Autoinkrementacja pamieci (kolejne wartosci z tablicy)
DMA2_Stream4->CR |= DMA_SxCR_CIRC; 
//Circular mode
DMA2_Stream4->CR |= DMA_SxCR_PSIZE_0 ; 
//Half-word dla peryferiow
DMA2_Stream4->CR |= DMA_SxCR_MSIZE_0; 
//Half-word dla pamieci
DMA2_Stream4->CR |= DMA_SxCR_EN; 
//Enable Stream5 
}

////////////////////////////////////////////////////////////////////////

//
piece of main
ADC1->CR2 |= ADC_CR2_SWSTART; 
//ADC enable
ADC1->CR2 |= ADC_CR2_DDS;
while
(1){
napiecie = buforADC[0] * 8059/10000;
temperatura = (1430 - buforADC[1] * 8059/10000)*10/43+25; Delay(50);
}

My problem is that values from buforADC[0] and buforADC[1] are mixing.Sometimes buforADC[1] has the value from buforADC[0] and so on.. I coulnd't find any solution on polish forums, so I try here. Sorry forry my poor english, hope to get some answers! Cheers!
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    November 7, 2014
    Posted on November 07, 2014 at 17:54

    I've posted some examples using the Standard Peripheral Library, the register level stuff is rather to time consuming for my tastes.

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..