Stm32f4 counting pulses (How can I adjust the rising edge voltage ?)
Hello all,
At the moment I use TIM2 on the stm32f4 - Discovery Board to count pulses (rising edges). How can I adjust the thresholds for the rising edges ? I want to count 1 V pulses. At the moment it is just possible to count 2V pulses.
Here is the code of my timer function.
If there is another way to count pulses really fast (interrupts are to slow) with an adjusted rising edge, please let me know.
void timer_2_pulse_counter_gpioa1_Init(){
RCC->AHB1ENR |= 0x01; // 1: IO port A clock enabled
//RCC->AHB1ENR |= 0x10; // 1: IO port E clock enabled
// APB1 peripheral reset register
RCC->APB1ENR |= 0x01; // 1: enable TIM2
// GPIO port mode register (GPIOx_MODER)
GPIOA->MODER |= 0x00000008; // 10: Alternate function mode PA1 => AF mode
GPIOA->AFR[0] |= 0x00000010; // 1000: Must refer to AF1 (alternate function for TIM1/ TIm2)
GPIOA->PUPDR |= 0x00000008; // Sets pull down resistor for PA1
// CCMR!: capture/compare mode register 1
TIM2->CCMR1 |= 0x0100; // CC2 channel is configured as input, IC2 is mapped on TI2
// SMCR: Slave Mode control register
TIM2->SMCR |= 0x0007; // Bits[2:0] 111: External Clock Mode 1 - Rising edges of the selected trigger clock the counter.
TIM2->SMCR |= 0x0060; // Bits[6:4] 110: selected Trigger: Filtered Timer Input 2 (TI2FP2)
TIM2->ARR = 0xFFFF; // Set the timer reset on the highest possible value
TIM2->CR1 |= 0x0001; //0001 Enable Timer
}Many thanks in advance for your support!