Skip to main content
melpel
Visitor II
May 20, 2015
Question

STM32F3xx and Ulink2 Debugger

  • May 20, 2015
  • 1 reply
  • 624 views
Posted on May 20, 2015 at 17:39

Using a ULink2 debugger I can download code OK, but debugging is marginal to non-functional.  I found if I press the hardware reset AFTER entering the ''Start Debug Session'', I can usually get 1-break point to work reasonably well.  I've heard the ULink2 should use an *.ini file for proper configuration to the application, but can find no details or examples or any information which would be in that ini file.  Suggestions...?

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    May 21, 2015
    Posted on May 21, 2015 at 03:11

    You probably want to double check you clock, pll, and flash state settings. It's going to run SystemInit() [system_stm32f3xx.c] prior to getting to your main() function, so ''run to main'' can get jammed up.

    I have to use .INI files if I want to run from RAM, as you have to ''LOAD'' the executable code rather than program the FLASH. Honestly don't think ones going to help you here.

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..