Skip to main content
keith23
Visitor II
September 28, 2016
Question

stm32f334 HRTIM

  • September 28, 2016
  • 1 reply
  • 578 views
Posted on September 28, 2016 at 15:29

I amusing the example program to run a single PWM and it works. All I am trying to do is run the CPU at a slower speed to conserve power. If I run it at 8Mhz with a pll setting of less the times 6 (so 48Mhz), the HRTIM will always timeout during calibration.

I have set the sysTick to give 1ms interrupts.

Is this a limitation of the HRTIM or is there something I can do?

    This topic has been closed for replies.

    1 reply

    slimen
    Visitor II
    September 28, 2016