Skip to main content
frackers
Senior
May 3, 2016
Question

STM32F303 PWM control via CubeMX HAL

  • May 3, 2016
  • 0 replies
  • 430 views
Posted on May 03, 2016 at 06:34

Greetings all

I'm using  HAL_TIM_PWM_ConfigChannel() to set the Pulse value for my PWM output but I want to modulate it (think IR LED on/off keying) so I'm currently using HAL_TIM_PWM_Start() and HAL_TIM_PWM_Stop(). The latter leaves the output in a high impedance state which causes the output to drift around falsely turning on a MOSFET driver. 

Can I directly manipulate the output using the GPIO registers or are they totally disabled due to the mode being set to GPIO_MODE_AF_PP (alternate function) or is there a recognised way I can do this with minimal overhead (preferably staying with the HAL)?

    This topic has been closed for replies.