Skip to main content
abhishekmathur
Associate
October 11, 2011
Question

STM32F10xxx DSP library FFT algorithm

  • October 11, 2011
  • 5 replies
  • 1374 views

Posted on October 11, 2011 at 12:34  Hi,

I am using STM32F10xxx DSP library (not the CMSIS DSP) algorithm for calculating FFT of an input sequence.

I want to know the order in which the input samples is expected by this algorithm and the order in which the output is given, eg:

 

If FFT of x[0] is X[0]

 

so if I give input as x[0],x[1],x[2],x[3] . . .

then will I get output as X[0],X[1],X[2],X[3] . . .

 

ie. input in natural order and output in natural order

ie. the algorithm has inbuilt bit reversal implemented.

OR the input and output should be in any other order.

 

Also,

I want to know that if by any means I can generate twiddle factors of my own then can I use the 64 point, 256 point and 1024 point algorithms for calculating FFT at higher points say 2048.??

 

#dsp-stm32f10xx-library

This topic has been closed for replies.

5 replies

infoinfo989
Associate III
October 12, 2011
Posted on October 12, 2011 at 07:10

You might find this interesting:

https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Complexreal, 1632bit, radix42 FFT, windowing, sqrt and magnitude library&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&currentviews=1762

abhishekmathur
Associate
October 12, 2011
Posted on October 12, 2011 at 09:43

Actually , my question is specificaly for the DSP library provided by STMicroelectronics.

Manual:

http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/USER_MANUAL/CD00208762.pdf

Different libraries implement algorithm in different ways . I am using the one provided by ST.

satishkumars
Visitor II
March 4, 2013
Posted on March 04, 2013 at 09:03

Hi Abhishek how did you implemnt the algorithm finally even i am to stuck in the same state what you were. Did you come to know the format for the input and output ?

denis
Associate III
October 9, 2013
Posted on October 09, 2013 at 14:57

question, where the heck is this library ?

STM32F10x DSPLib

Tesla DeLorean
Guru
October 9, 2013