Skip to main content
ioannis2
Associate II
May 17, 2013
Question

STM32F10x DSP library, where is it?

  • May 17, 2013
  • 3 replies
  • 876 views
Posted on May 17, 2013 at 09:48

I looking for a download link of the STM32F10x DSP Library, there multiple references to it and a user manual (UM0585) but cannot find the actual code anywhere... Anyone?

    This topic has been closed for replies.

    3 replies

    frankmeyer9
    Associate III
    May 17, 2013
    Posted on May 17, 2013 at 13:49

    It is at least explicitely available for ST's M4 cores, say, the F3 and the F4, where you can download it as STM32Fxxx_DSP_StdPeriphLib_Vxxx.

    The DSP part is provided by ARM, and can be used/compiled for M0, M3 and M3 cores.

    Perhaps ST doesn't see DSP-like applications as a primary market for the F1xx series

    ioannis2
    ioannis2Author
    Associate II
    May 20, 2013
    Posted on May 20, 2013 at 11:34

    Well, I have inherited a project that uses the fore mentioned library but modified without explicit comments...The original lib is actually written by ST and is in assembly. I need to get my hands on the  original lib so I can do a diff to evaluate the modifications that have been performed... I suppose it must have been moved to the legacy staff, but nevertheless I need access to it.

    Anybody?

    zzdz2
    Associate
    May 20, 2013
    Posted on May 20, 2013 at 12:56

    It looks like I never installed it but the installer itself is still on my drive, file attached.

    ________________

    Attachments :

    um0585.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0r7&d=%2Fa%2F0X0000000beW%2FlGmMORuX2BlUJRcE2BLkDhbyvetWUgfKAjYulaCMOn4&asPdf=false