Skip to main content
jefferson
Visitor II
October 24, 2014
Question

STM32F103R4 CAN PA11 PA12

  • October 24, 2014
  • 1 reply
  • 631 views
Posted on October 24, 2014 at 17:45

Hello,

I had tried to set the ''CAN BUS'' in MCU STM32F103R4 in PA11 and PA12 with STM libraries, but when i try to transmit any message, the MCU don´t transmit, Someone could help me with the module configuration? 

Thanks.
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    October 24, 2014
    Posted on October 24, 2014 at 18:19

    CAN needs to transmit to something which is capable of sinking and acknowledging the data.

    Have you looked over the examples?

    STM32F10x_StdPeriph_Lib_V3.5.0\Project\STM32F10x_StdPeriph_Examples\CAN\
    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..