Question
STM32F070 Tamper and Periodic WakeUp
Posted on January 05, 2016 at 11:29
Hi all.
I'm getting in trouble with STM32F070 RTC-based features availability.Is the periodic wake-up on RTC feature available?Reading datasheet and on-line feature description seems that is present, but HAL documentations UM1785 says '' Not available on F030x4/x6/x8 and F070x6 '' on '' RTC Wake-up configuration '' (pag. 373).Is the tamper detection feature available?There are no RTC_Tamper examples on HAL Example library for STM320F070, but there are for STM32F072.Many thanks for helpLuigi