Question
STM32F030K6 Exit from sleep and stop mode
Posted on December 10, 2015 at 10:23
Hi. Exit from sleep and stop mode not work. When STM32 in sleep mode and push to buttons on pins PA0, PA1, PA2, PA5, PA6, PA7, PA13 (low or high level) STM32 don't exit from sleep mode.
sleep_counter++; if((sleep_counter>=400000)&&(lamp_start==0)) { GPIO_ResetBits(GPIOF, GPIO_Pin_0); //A GPIO_ResetBits(GPIOF, GPIO_Pin_1); //B GPIO_ResetBits(GPIOA, GPIO_Pin_3); //C GPIO_ResetBits(GPIOB, GPIO_Pin_1); //D GPIO_ResetBits(GPIOA, GPIO_Pin_9); //E GPIO_ResetBits(GPIOA, GPIO_Pin_10); //F GPIO_ResetBits(GPIOA, GPIO_Pin_13); //G GPIO_SetBits(GPIOA, GPIO_Pin_14); //DP PWR->CSR = PWR_CSR_EWUP1 | PWR_CSR_EWUP2 | PWR_CSR_EWUP5 | PWR_CSR_EWUP6 | PWR_CSR_EWUP7; RTC_AlarmTypeDef RTC_AlarmStructure; RTC_SetAlarm(RTC_Format_BIN, RTC_Alarm_A, &RTC_AlarmStructure); RTC_ITConfig(RTC_IT_ALRA, ENABLE); RTC_AlarmCmd(RTC_Alarm_A, ENABLE); PWR_WakeUpPinCmd(PWR_WakeUpPin_1,ENABLE); sleep_counter=0; // Clear Wakeup flag PWR->CR |= PWR_CR_CWUF; // Select STANDBY mode PWR->CR |= PWR_CR_PDDS; // Set SLEEPDEEP bit of Cortex-M0 System Control Register SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk; // Request Wait For Interrupt __WFI(); }