Skip to main content
markjohnson9
Associate III
January 26, 2016
Question

STM32F030 TIM3

  • January 26, 2016
  • 1 reply
  • 480 views
Posted on January 26, 2016 at 01:51

Does anyone know if its possible to output TIM3 on an I/O pin to view or trigger another external device? I noticed the absence of the BDTR register for TIM3 and the MOE bit in the register map bit fields. If there another  method which a TIM3 register should be used to output a signal on an I/O pin?

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    January 26, 2016
    Posted on January 26, 2016 at 02:15

    Yeah, pretty sure you just put it in Output Compare, or PWM1/PMW2 mode. It is not a ''special'' timer like TIM1/TIM8, so no PWM Output Enable required, or Break features

    Check the TIM3_CHx pins for your specific device configuration

    http://www.st.com/web/en/resource/technical/document/datasheet/DM00088500.pdf

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..