STM32CubeMX STM32F0xx_StdPeriph_Lib_V1.5.0 This package Version is not managed
The package version is not managed on this version of STM32CubeMX
stm32f0_stdperiph_lib.zip -> STM32F0xx_StdPeriph_Lib_V1.5.0 Firmware package STM32F0xx_StdPeriph_Lib_V1.5.0 and STM32CubeMX 4.11.0 - Error happensHello,
When I started a library install on Help->Install New Libraries->From Loc (STM32CubeMX 4.11.0 ..and 4.10. too/same situation) at the end of the ''unzip''/install process,
occur an error: The package version is not managed on this version of STM32CubeMXI would like install/update to STM32F0xx_StdPeriph_Lib_V1.5.0
(I have freezing problems on HAL_UART_Receive_IT, eventually this new library will be solving..) the STM32F0xx_StdPeriph_Lib_V1.3.0 is installed in the STM32CubeMX 4.11.0. On the STM32CubeMX I saw that only the STM32F0xx standard peripherals library 1.4.0 version was on list. Where is this file/1.4.0 version to download on ST/Site? What's going on STM32CubeMX 4.11.0 and STM32F0xx_StdPeriph_Lib_V1.5.0 due these files were fresh downloaded from ST/Links? Help, please ..!STM32CubeMX 4.11.0
http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1533/PF259242?sc=stm32cube
http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1533/PF259242?sc=stm32cube
#stm32f0_stdperiph_lib.zip -> STM32F0xx_StdPeriph_Lib_V1.5.0
http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1939/PF257884
http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1939/PF257884
#