Skip to main content
YOEL BEN NAIM
Associate
April 20, 2017
Question

STM32756G-EVAL SPI/I2C

  • April 20, 2017
  • 2 replies
  • 722 views
Posted on April 20, 2017 at 11:19

Hi

I want to connect a thermal camera to the STM32756G-EVAL EV board.

In order to connect it I need to have one free SPI terminal and one I2C free terminal.

When looking at the user manual I can't find SPI mentioned anywhere, and if I look at the SPI ports of the Microcontroller it seems that they are taken by other IC's and peripherals. Same for the I2C ports.

What do I do?

How can I connect I2C and SPI to the 

STM32756G-EVAL EV board?

Thank you

#stm32756g-eval-spi/i2c
This topic has been closed for replies.

2 replies

Technical Moderator
April 20, 2017
Posted on April 20, 2017 at 14:33

Hi

ben_naim.yoel

,

You should refer to the

http://www.st.com/content/ccc/resource/technical/document/datasheet/fb/d4/56/db/60/61/4f/9c/DM00166pdf/files/DM00166pdf/jcr:content/translations/en.DM00166pdf

to have idea aboutthe features, the list of peripherals availableand to be able identify the pins assignment (free/usable pins)

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Max
ST Employee
April 21, 2017
Posted on April 21, 2017 at 07:05

This is true that the EVAL board is quite crowded and most of the pins are used on the board.

You should identify a function you are not using on the board and remove the 0 Ohm resistor that connect the pin to the board function.

This way, the pin becomes available for your own usage.

In some (rare) cases you may even have a jumper to disconnect the on-board function: look at the board schematic to identify those.