Question
STM32091C-Eval Board
Posted on January 18, 2018 at 15:28
I am working with the STM32091C-Eval board trying to see how the touch pads work. I have selected the TSC example code and gone to build the code using TrueStudio. I receive the following error message:
08:27:19 **** Rebuild of configuration Debug for project STM32091C_EVAL ****
Info: Internal Builder is used for buildarm-atollic-eabi-gcc -c ..\..\..\..\..\..\..\..\Drivers\STM32F0xx_HAL_Driver\Src\stm32f0xx_hal_rcc_ex.c -mthumb -mcpu=cortex-m0 -std=gnu11 -DSTM32F091xC -DUSE_HAL_DRIVER -DUSE_STM32091C_EVAL -I../../../Inc -I../../../../../../../../Drivers/CMSIS/Device/ST/STM32F0xx/Include -I../../../../../../../../Drivers/STM32F0xx_HAL_Driver/Inc -I../../../../../../../../Drivers/BSP/STM32091C_EVAL -I../../../../../../../../Drivers/BSP/Components/Common -I../../../../../../../../Utilities/Log -I../../../../../../../../Utilities/CPU -I../../../../../../../../Drivers/CMSIS/Include -Os -ffunction-sections -g3 -fstack-usage -Wall -fmessage-length=0 -Wno-strict-aliasing -specs=nano.specs -o Drivers\STM32F0xx_HAL_Driver\stm32f0xx_hal_rcc_ex.o arm-atollic-eabi-gcc: error: ..\..\..\..\..\..\..\..\Drivers\STM32F0xx_HAL_Driver\Src\stm32f0xx_hal_rcc_ex.c: No such file or directoryarm-atollic-eabi-gcc: fatal error: no input filescompilation terminated.The file is in the code display under STM32F0xx_HAL_Driver and I found the location of the code on my hard drive. I don't know why I have the error.