Skip to main content
hpipon957
Associate III
July 7, 2010
Question

STM32 - uTasker project update

  • July 7, 2010
  • 3 replies
  • 722 views
Posted on July 07, 2010 at 23:50

STM32 - uTasker project update

    This topic has been closed for replies.

    3 replies

    lowpowermcu
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:57

    Hi mjbcswitzerland,

    I have tried to test this tool but when I started filling the ''µTasker license request formular'' I didn't find STM32 port.

    Only STR9, luminary, AT, AVR and LPC. How could I proceed ?

    Thanks in advance.

    Regards,

    lowpower.

    hpipon957
    hpipon957Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:57

    Hi All

    So that you can get a better idea of the project a video had been added here:

    http://www.youtube.com/watch?v=2Rbz1SOoJVI

    I hope that you enjoy it.

    Regards

    Mark

    hpipon957
    hpipon957Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:57

    Hi lowpower

    Presently there is only an executable (simulator) and binary demo of the new STM32 project and no developers' package as such. These can be downloaded and tested by anyone at the given link - the project (developers' package) will be made available in the near future but there is still some work involved (like documentation, USB and an IPv4/v6 dual-stack which will be included in the next releases).

    Note that there are several projects available ranging from Coldfire through AVR32, ARM7, ARM9 and various Cortex M3 parts - the STM32 will become the main ST focus since it is nice chip (in the targeted device class) and the STR91XF project will be phased out (i.e. generally no further active development).

    If you have real interests in a Beta version for your tests please contact me at the ''info'' address on the uTasker web site because this can certainly be arranged for serious users.

    Cheers

    Mark

    http://www.utasker.com/