Skip to main content
llamka
Associate
April 11, 2014
Question

STM32 Nucleo - Linux support

  • April 11, 2014
  • 3 replies
  • 1125 views
Posted on April 11, 2014 at 13:09

Hello,

I am trying to use STM32 Nucleo board under Linux (tried Ubuntu 12.04 and 13.10). After connecting, a mass storage and ACM devices appear, mass storage for firmware uplading works, but I can't get the ACM device (located at /dev/ttyACM0) to work with any baud rate. Am I doing something wrong or it's because the virtual COM port is somehow proprietary? If it's the latter, is there any chance that Linux will be supported in future?

Thanks,

Jan
    This topic has been closed for replies.

    3 replies

    frankmeyer9
    Associate III
    April 11, 2014
    Posted on April 11, 2014 at 14:04

    A rights issue ?

    Have you tried as root, or with sudo ?

    If that works, you probably need to add your ''user'' to the dialout group.

    llamka
    llamkaAuthor
    Associate
    April 11, 2014
    Posted on April 11, 2014 at 16:48

    Nope, it doesn't seem like a rights issue, I am running the command as root. Can you confirm that Nucleo works on Linux? If so, I'll try to dig into it deeper, but I had no luck with it on two different machines.

    frankmeyer9
    Associate III
    April 11, 2014
    Posted on April 11, 2014 at 18:47

    Can you confirm that Nucleo works on Linux?

     

    No, I can't - because I do not have any Nucleo board, and thus can't try.

    However, if the /dev/ACM0 device is present, the board is supposedly recognized as USB ACM device. That does not mean that it is fully compliant. Can you remember the totally broken STLink-V1 implementation ? It wouldn't be the first time ST tested only on Windows machines.

    Perhaps some further investigation/testing

    https://www.kernel.org/doc/Documentation/usb/acm.txt

    can help you further ...