Skip to main content
sergalyant
Associate
December 19, 2014
Question

STM32 isochronous transfer

  • December 19, 2014
  • 0 replies
  • 446 views
Posted on December 19, 2014 at 08:33

how to transfer 512 bytes?

Send_DATA ((unsigned 
char
*)trBuffer, 512);

void
Send_DATA(uint8_t* ptrBuffer, uint16_t Send_length)
{
if
(GetENDPOINT(ENDP1) & EP_DTOG_RX) 
// NOT TX ie SW_BUF
{
UserToPMABufferCopy(ptrBuffer, ENDP1_BUF0ADDR, Send_length);
SetEPDblBuf0Count(ENDP1, EP_DBUF_IN, Send_length);
}
else
{
UserToPMABufferCopy(ptrBuffer, ENDP1_BUF1ADDR, Send_length);
SetEPDblBuf1Count(ENDP1, EP_DBUF_IN, Send_length);
}
FreeUserBuffer(ENDP1, EP_DBUF_IN); 
// Toggles EP_DTOG_RX / SW_BUF
SetEPTxValid(ENDP1);
packet_sent = 0;
}
Send_DATA ((unsigned 
char
*)trBuffer, 512);

buffer is set to isochronous mode

/* Initialize Endpoint 1 (TX) (IN) (EP1_IN)*/
SetEPType(ENDP1, EP_ISOCHRONOUS);
SetEPDoubleBuff(ENDP1);
SetEPDblBuffAddr(ENDP1, ENDP1_BUF0ADDR, ENDP1_BUF1ADDR);
SetEPDblBuffCount(ENDP1, EP_DBUF_IN, 0x200);
ClearDTOG_TX(ENDP1); 
// USB PERIPHERAL
ClearDTOG_RX(ENDP1); 
// SW_BUF for APPLICATION
ToggleDTOG_RX(ENDP1); 
// NOT TX ie SW_BUF
SetEPTxStatus(ENDP1, EP_TX_NAK);
SetEPRxStatus(ENDP1, EP_RX_DIS); 
// NOT TX DISABLE

endpoint

/* Endpoint 1 - Standard Descriptor */
0x09, 
/* bLength */
USB_ENDPOINT_DESCRIPTOR_TYPE, 
/* bDescriptorType */
0x81, 
/* bEndpointAddress 1 in endpoint*/
0x05, 
/* bmAttributes */
0x00, 
/* wMaxPacketSize 512 bytes*/
0x02,
0x01, 
/* bInterval */
0x00, 
/* bRefresh */
0x00, 
/* bSynchAddress */

what I'm doing wrong?
    This topic has been closed for replies.