Skip to main content
SYako
Associate III
December 17, 2021
Solved

STM32 external OPAMPx_VINM pins

Hi, I'm working on a project which involves STM32L476QEI. It has external dedicated OPAMP1_VINM and OPAMP2_VINM (M3 and M4 pins). If I'm not going to use the opamp functionality, do I have to connect them to the ground or leave them floating? What I learn from CubeMX is that I can use them to remap connections to free up GPIO. Are there other possibilities that I missed?

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
December 20, 2021

When not in use, I would recommend to connect them on GND, even if these are not digital inputs with Schmitt trigger. In the case of the BGA132, these are dedicated pins in order to minimize the bias current (see RM0351, section 23.3.3):

The dedicated pin is only available on BGA132 and BGA169 [...] package. This configuration provides the lowest input bias current (see datasheet).

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
December 20, 2021

When not in use, I would recommend to connect them on GND, even if these are not digital inputs with Schmitt trigger. In the case of the BGA132, these are dedicated pins in order to minimize the bias current (see RM0351, section 23.3.3):

The dedicated pin is only available on BGA132 and BGA169 [...] package. This configuration provides the lowest input bias current (see datasheet).

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.