Question
STM32 5V tolerant I/O ?
Posted on November 25, 2012 at 11:22
I'm sorry, but I do not quite 5v tolerant ports for STM32
. I do not unterstand concept ''Total injected current (sum of all I/O and control pin)''
Example STM32F0 and on 8 5V tolerant I/O connected LED with resistor powered from +5V (resistor limit current of every LED on max 5mA). After reset is I/O configured as input. What current will flow through the I/Oport from 5V over
LED
+ R? It
injection current and
exceed this design Total injected current 25mA? InIn
RM0091
Reference manual page 121 read protection diode on FT ''
VDD_FT is a potential specific to five-volt tolerant I/Os and different from VDD''. W
here the
potential
at the cathode
takes?
I/O switched, on Output with open drain (No pull-up, pull-down), if port is set on 0 LED light and current to I/O is 8x5mA.