Question
STLink V2 on STM32F4 Discovery
Posted on February 26, 2014 at 11:17
Hello,
I have a STM32F4 Discovery. It has an on-board STLink V2 debugger that programs/debug the STM32F407 micro. I'm develloping a circuit that has also a STM32 micro and I would like to know if I can use the STLink embedded in the discovery kit to program the STM32 in the PCB I'm designing, making the appropriate soldering/desoldering solder jumpers in the discovery kit.A more embracing question: embedded STLink-V2 on discovery kit (STM32F4DISCO) can be used to program/debug any external application with STM32 micro that supports SWD interface, like STM32L151 or STM32K058?Best regards,Vitor Barbosa #debug-stm32-using-st-link/v2