Question
ST-Link upgrade
Posted on December 01, 2014 at 15:56
I am using stm32fvldiscovery card and Kiel uv4.
Flash download fails with dll fail messages ( these are different today to yesterday) But when I ran a kiel provided STlinkupgrade.exe it reported old firmware version V8.J17.S23 should be upgraded to V2.J16.SO. But the upgrade fails. So now I have installed the STM supplied utilities. These connect and show the card details and give the warning ST-LINK Firmware version : V1J12S0 (Need Update) Old ST-LINK firmware detected! But when I run the ST-LINK->Firmware update menu item it can not connect. No St-Link device detected. Which is odd as exiting this back to the main util screen it connects just fine. I have tried many versions of unplugging the usb cable, and holding down the black reset button, but no change. How do I update the firmware? #stm32fvldiscovery-st-link-upgrad