Skip to main content
Associate
January 2, 2024
Question

SMT32F407VGT6 / CAN issue

  • January 2, 2024
  • 2 replies
  • 1419 views

主控板 (SMT32F407VGT6)与同服板 (STM32F407VGT6) 之间的CAN通讯,环境温度低于-10度,通讯不正常,环境温度高过-10度!

2 replies

mƎALLEm
Technical Moderator
January 2, 2024

Hello @JACK00 ,

In next time, could you please describe your issue in English as other community members can help you?

Translation:

"The CAN communication between the main control board (SMT32F407VGT6) and the server board (STM32F407VGT6), the ambient temperature is lower than -10 degrees, the communication is abnormal, and the ambient temperature is higher than -10 degrees!"

Not sure the question is clear. Could you please elaborate more?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
JACK00Author
Associate
January 2, 2024

The CAN communication between the main control board (SMT32F407VGT6) and the same server board (STM32F407VGT6) shows that the ambient temperature is below -10 degrees, the communication is abnormal, and the ambient temperature is above -10 degrees! Immediately returning to normal, may I ask what the reason is? Confirm that the CAN communication interface hardware chip meets the requirements!

mƎALLEm
Technical Moderator
January 29, 2024

What is your clock source? HSI or HSE?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
January 2, 2024
Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..