Skip to main content
smrtkai
Associate III
April 13, 2016
Question

SDRAM on STM32F429I with disabled 16-bit byte

  • April 13, 2016
  • 3 replies
  • 765 views
Posted on April 13, 2016 at 12:37

Hi,

I am using a STM32F429I discovery board. I have a running project in which I can generate code from STM32CubeMX. I would like to disable ''16-bit byte'', because I need the pin PE0 as a clock source for TIM4 (ETR2).

The FMC controller for SDRAM2 is configured as follows:

Clock and chip enable: SDCKE1+SDNE

Internal bank numer: 4 banks

Address: 13 bits

Data: 16 bits

16-bit byte enable

Does anyone knows if this is possible?
    This topic has been closed for replies.

    3 replies

    slimen
    Visitor II
    April 14, 2016
    Posted on April 14, 2016 at 14:22

    Hello,

    Using CubeMX, it's possible to disable ''16-bit byte'' and enable the pin PE0 as a clock source for TIM4 (ETR2).

    I hope that answer your question, else you can provide more information about your issue.

    Regards

    -ForumSTM32-
    scott23
    Visitor II
    April 14, 2016
    Amel NASRI
    Technical Moderator
    April 14, 2016
    Posted on April 14, 2016 at 15:23

    Hi jisa.sana,

    The provided link is out of topic I think.

    -Mayla-

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.