Skip to main content
DPRAJ.1
Associate
November 9, 2020
Question

SDRAM interfacing issue

  • November 9, 2020
  • 3 replies
  • 1838 views

I am using 12.1" TFT Display of 800x600 resolution and interfacing it with STM32F429BI Micro-controller and IS42S16400J SDRAM .I am getting the flickering issue in my display. When i by pass the SDRAM it working ok , there is no flickering, but on connecting through SDRAM it starts giving flickering issue.

Video of above mentioned problems is attached.

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
November 9, 2020

Unless the video has details about the memory interface, width and speed settings I'm not sure watching it will help me.

Post the details about SDRAM and LTDC settings.

I​s the memory 32-bit wide?

Have you tried reducing the colour depth. How about pixel clock or refresh rate? What are the display specs and parameters?

800x600 is close to bandwidth ceiling​

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
DPRAJ.1
DPRAJ.1Author
Associate
November 9, 2020

Below mentioned are the details you said.

refresh count is 1386

void SystemClock_Config(void)

{

 RCC_OscInitTypeDef RCC_OscInitStruct;

 RCC_ClkInitTypeDef RCC_ClkInitStruct;

 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct;

 __PWR_CLK_ENABLE();

 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE|RCC_OSCILLATORTYPE_LSE;

 RCC_OscInitStruct.HSEState = RCC_HSE_ON;

 RCC_OscInitStruct.LSEState = RCC_LSE_ON;

 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;

 RCC_OscInitStruct.PLL.PLLM =4;// 5;

 RCC_OscInitStruct.PLL.PLLN =180;//144; //225;

 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;

 RCC_OscInitStruct.PLL.PLLQ = 4;

 HAL_RCC_OscConfig(&RCC_OscInitStruct);

 HAL_PWREx_ActivateOverDrive();

 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_SYSCLK|RCC_CLOCKTYPE_PCLK1

               |RCC_CLOCKTYPE_PCLK2;

 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;

 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV4;

 HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5);

 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_LTDC|RCC_PERIPHCLK_RTC;

 PeriphClkInitStruct.PLLSAI.PLLSAIN =144;//201;//146; //181;

 PeriphClkInitStruct.PLLSAI.PLLSAIR = 4;//2;

 PeriphClkInitStruct.PLLSAIDivR = RCC_PLLSAIDIVR_4;//8;

 PeriphClkInitStruct.RTCClockSelection = RCC_RTCCLKSOURCE_LSE;

 HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct);

 HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);

 HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);

 /* SysTick_IRQn interrupt configuration */

 HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);

}

void MX_LTDC_Init(void)

{

LTDC_LayerCfgTypeDef pLayerCfg;

 hltdc.Instance = LTDC;

 hltdc.Init.HSPolarity =LTDC_HSPOLARITY_AH;// LTDC_HSPOLARITY_AL;

 hltdc.Init.VSPolarity = LTDC_VSPOLARITY_AL;//LTDC_VSPOLARITY_AL;

 hltdc.Init.DEPolarity =LTDC_DEPOLARITY_AL; //LTDC_DEPOLARITY_AL;

 hltdc.Init.PCPolarity = LTDC_PCPOLARITY_IPC;

 hltdc.Init.HorizontalSync = 40;

 hltdc.Init.VerticalSync = 9;

 hltdc.Init.AccumulatedHBP = 42;

 hltdc.Init.AccumulatedVBP = 11;

 hltdc.Init.AccumulatedActiveW = 1054;

 hltdc.Init.AccumulatedActiveH = 664;

 hltdc.Init.TotalWidth = 1056;

 hltdc.Init.TotalHeigh = 666;

 hltdc.Init.Backcolor.Blue = 0;

 hltdc.Init.Backcolor.Green = 0;

 hltdc.Init.Backcolor.Red = 0;

 HAL_LTDC_Init(&hltdc);

 pLayerCfg.WindowX0 = 0;

 pLayerCfg.WindowX1 = 800;//800;//240;

 pLayerCfg.WindowY0 = 0;

 pLayerCfg.WindowY1 = 600;//320;//160;

 pLayerCfg.PixelFormat = LTDC_PIXEL_FORMAT_RGB565;

 pLayerCfg.Alpha = 255;

 pLayerCfg.Alpha0 = 0;

 pLayerCfg.BlendingFactor1 = LTDC_BLENDING_FACTOR1_PAxCA;

 pLayerCfg.BlendingFactor2 = LTDC_BLENDING_FACTOR2_PAxCA;

 pLayerCfg.FBStartAdress = SDRAM_DEVICE_ADDR;//(uint32_t)&Color;

 pLayerCfg.ImageWidth = 800;

 pLayerCfg.ImageHeight = 600;

 pLayerCfg.Backcolor.Blue = 0;

 pLayerCfg.Backcolor.Green = 0;

 pLayerCfg.Backcolor.Red = 0;

 HAL_LTDC_ConfigLayer(&hltdc, &pLayerCfg, 0);

}

void MX_FMC_Init(void)

{

 FMC_SDRAM_TimingTypeDef SdramTiming;

 /** Perform the SDRAM1 memory initialization sequence

 */

 hsdram1.Instance = FMC_SDRAM_DEVICE;

 /* hsdram1.Init */

 hsdram1.Init.SDBank = FMC_SDRAM_BANK2;

 hsdram1.Init.ColumnBitsNumber = FMC_SDRAM_COLUMN_BITS_NUM_8;

 hsdram1.Init.RowBitsNumber = FMC_SDRAM_ROW_BITS_NUM_12;//FMC_SDRAM_ROW_BITS_NUM_11;

 hsdram1.Init.MemoryDataWidth = FMC_SDRAM_MEM_BUS_WIDTH_16;

 hsdram1.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_4;

 hsdram1.Init.CASLatency = FMC_SDRAM_CAS_LATENCY_3;//FMC_SDRAM_CAS_LATENCY_1;

 hsdram1.Init.WriteProtection = FMC_SDRAM_WRITE_PROTECTION_DISABLE;

 hsdram1.Init.SDClockPeriod = FMC_SDRAM_CLOCK_PERIOD_2;

 hsdram1.Init.ReadBurst = FMC_SDRAM_RBURST_DISABLE;

 hsdram1.Init.ReadPipeDelay = FMC_SDRAM_RPIPE_DELAY_1;//FMC_SDRAM_RPIPE_DELAY_0;

 /* SdramTiming */

/* SdramTiming.LoadToActiveDelay = 16;

 SdramTiming.ExitSelfRefreshDelay = 16;

 SdramTiming.SelfRefreshTime = 16;

 SdramTiming.RowCycleDelay = 16;

 SdramTiming.WriteRecoveryTime = 16;

 SdramTiming.RPDelay = 16;

 SdramTiming.RCDDelay = 16;*/

SdramTiming.LoadToActiveDelay  = 2;

 /* TXSR: min=70ns (7x11.11ns) */

 SdramTiming.ExitSelfRefreshDelay = 14;//7;

 /* TRAS: min=42ns (4x11.11ns) max=120k (ns) */

 SdramTiming.SelfRefreshTime   = 14;//4;

 /* TRC: min=70 (7x11.11ns) */

 SdramTiming.RowCycleDelay    = 14;//7;

 /* TWR: min=1+ 7ns (1+1x11.11ns) */

 SdramTiming.WriteRecoveryTime  = 2;

 /* TRP: 20ns => 2x11.11ns*/

 SdramTiming.RPDelay       = 4;//2;

 /* TRCD: 20ns => 2x11.11ns */

 SdramTiming.RCDDelay       = 4;//2;

 HAL_SDRAM_Init(&hsdram1, &SdramTiming);

 BSP_SDRAM_Initialization_sequence(REFRESH_COUNT);

}

void BSP_SDRAM_Initialization_sequence(uint32_t RefreshCount)

{

 __IO uint32_t tmpmrd =0;  

 /* Step 1: Configure a clock configuration enable command */

 Command.CommandMode       = FMC_SDRAM_CMD_CLK_ENABLE;

 Command.CommandTarget      = FMC_SDRAM_CMD_TARGET_BANK2;

 Command.AutoRefreshNumber    = 1;

 Command.ModeRegisterDefinition = 0;

 /* Send the command */

 HAL_SDRAM_SendCommand(&hsdram1, &Command, SDRAM_TIMEOUT);

 /* Step 2: Insert 100 us minimum delay */ 

 /* Inserted delay is equal to 1 ms due to systick time base unit (ms) */

 HAL_Delay(1);

 /* Step 3: Configure a PALL (precharge all) command */ 

 Command.CommandMode       = FMC_SDRAM_CMD_PALL;

 Command.CommandTarget      = FMC_SDRAM_CMD_TARGET_BANK2;

 Command.AutoRefreshNumber    = 1;

 Command.ModeRegisterDefinition = 0;

//// /* Send the command */

 //HAL_SDRAM_SendCommand(&hsdram1, &Command, SDRAM_TIMEOUT);  

HAL_SDRAM_SendCommand(&hsdram1, &Command, SDRAM_TIMEOUT); 

////  

// /* Step 4: Configure an Auto Refresh command */ 

 Command.CommandMode       = FMC_SDRAM_CMD_AUTOREFRESH_MODE;

 Command.CommandTarget      = FMC_SDRAM_CMD_TARGET_BANK2;

 Command.AutoRefreshNumber    = 4;

 Command.ModeRegisterDefinition = 0;

//// /* Send the command */

 HAL_SDRAM_SendCommand(&hsdram1, &Command, SDRAM_TIMEOUT);

////  

// /* Step 5: Program the external memory mode register */

 tmpmrd = (uint32_t)SDRAM_MODEREG_BURST_LENGTH_1     |

          SDRAM_MODEREG_BURST_TYPE_SEQUENTIAL  |

          SDRAM_MODEREG_CAS_LATENCY_3      |

          SDRAM_MODEREG_OPERATING_MODE_STANDARD |

           SDRAM_MODEREG_WRITEBURST_MODE_SINGLE;

  

 Command.CommandMode       = FMC_SDRAM_CMD_LOAD_MODE;

 Command.CommandTarget      = FMC_SDRAM_CMD_TARGET_BANK2;

 Command.AutoRefreshNumber    = 1;

 Command.ModeRegisterDefinition = tmpmrd;

//// /* Send the command */

 HAL_SDRAM_SendCommand(&hsdram1, &Command, SDRAM_TIMEOUT);

////  

//// /* Step 6: Set the refresh rate counter */

//// /* Set the device refresh rate */

 HAL_SDRAM_ProgramRefreshRate(&hsdram1, RefreshCount); 

}

DPRAJ.1
DPRAJ.1Author
Associate
November 10, 2020

Hey,

any suggestion or solution for this problem?