Question
SDIO timeout in DMA mode
Posted on January 11, 2016 at 01:02
Hi
In my application (STM32L4) I need to write two file for totally 400kB/s and I can't loss data (from ADC)In some speed test I obtain about 10MB/s, so theoretically there are no problem (I use a very good uSD with write speed=80MB/s)The write routine use two big buffer (one for file), every half and full buffer interrupt I write in DMA mode on SD.The write function of 20kB (I use FATFS) occupy CPU for 1-5ms, but in rare case (probably after error on SD?) this function last 100-200ms and so I loss data becouse the buffer filling is more faster.I can not afford itTo solve this problem I modify HAL_SD_CheckWriteOperation() that must be call afterHAL_SD_WriteBlocks_DMA()I changed the default timeout control (there was a terrible decreasing variable) with 35ms on systick. In case of error I return timeout errorUnfortunately FATFS haven't a re-write control after timeout error, so I want to create a trasparent re-write sistem in case of error.I work in BSP_SD_WriteBlocks_DMA()I tried to call those functions after a timeout error-HAL_SD_StopTransfer()
-Clear all flag
-Clear all interrupt
-SD_DMA_Congif()
-HAL_SD_WriteBlocks_DMA()
-HAL_SD_CheckWriteOperation()
But unfortunately not work: the HAL_SD_WriteBlocks_DMA() return CTIMEOUT.Probably the SD is in error or yet busy?I hope is possible find a solutionSomeone have ideas?My problem is resolvable?thanks #dma #sdio #timeout