Question
SDHC SPI STM32 Definitive Question
Posted on January 26, 2016 at 23:53
Hey everybody. I`ve been browsing the forum for a while trying to solve my problems with SDHC, but I can't find an answer. I have this 4gb SDHC card and it won't initialize at all! I just can't make it work. It works fine up to the CMD8, but when it comes to sending CMD55 and CMD41, the response is only a bunch of 0xFF. Has anyone developed this driver that could give me some help? I NEED to use the SPI interface.
I am using the STM32F105 and debuggin with the STM3210C-EVAL.Thank you! :D #stm32-sdhc-sd-card-stm3210c-eval