Skip to main content
Uwe Bonnes
Chief
September 23, 2016
Question

RM410: Documentation mismatch

  • September 23, 2016
  • 1 reply
  • 431 views
Posted on September 23, 2016 at 15:16

To whom it may concern,

RM0410 (DocID028270 Rev 2) for the STM32F76x tells on page 1484 in Table 258 about ''26 filter banks shared between CAN1 and CAN2'', while there are 28 registers and 28 banks in other devices. Probably the ''26'' is a typo.

#stm32f76
This topic has been closed for replies.

1 reply

Walid FTITI_O
Visitor II
November 10, 2016
Posted on November 10, 2016 at 11:22

Hi bonnes.uwe, 

Yes we confirm that this is an issue in the RM0410. We need to update total filter number for CAN1 and CAN2 (26 to 28). And the possible value for Bits 13:8 CANSB[5:0]: are 0..27

Thanks for the feedback.

-Hannibal-