Skip to main content
Andrei Chichak
Lead
May 30, 2017
Question

Request for enhancement : Cube 4.21.0

  • May 30, 2017
  • 1 reply
  • 416 views
Posted on May 30, 2017 at 19:11

Eric,

In the implementation that was included in 4.21 there was a couple of MISRA violations inserted.

Unlike the assert_failed routine, _Error_Handler uses char* and int for parameters instead of uint8_t* and uint32_t.

Just a head-up.

Also, the USER CODE BEGIN and USER CODE END comments have an incorrect function name.

Andrei

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    May 30, 2017
    Posted on May 30, 2017 at 22:49

    Hi

    Chichak.Andrei

    ,

    Thank you for your reported issue.

    I will forward your request internally to our CubeMx team.

    Thanks

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks