Associate
June 8, 2011
Question
Read pressure sensor with I2C in master receiver mode
- June 8, 2011
- 0 replies
- 598 views
Posted on June 08, 2011 at 10:12
Hi All,
Need some advise here with I2C. I'm trying to use I2C in master receiver mode to read two bytes of data out of a pressure sensor. The required command sequence is pg 8 of attached data sheet. Here is the code: GPIO_InitTypeDef GPIO_InitStructure; /* SDA */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_OD; GPIO_Init(GPIOB, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_OD; GPIO_Init(GPIOB, &GPIO_InitStructure); I2C_InitTypeDef I2C_InitStructure; /* I2C configuration */ I2C_InitStructure.I2C_Mode = I2C_Mode_I2C; I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2; I2C_InitStructure.I2C_OwnAddress1 = I2C1_SLAVE_ADDRESS7; I2C_InitStructure.I2C_Ack = I2C_Ack_Enable; I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_InitStructure.I2C_ClockSpeed = I2C_Speed; I2C_Cmd(I2C1, ENABLE); I2C_Init(I2C1, &I2C_InitStructure); int sensor_data[2]; sensor_data[0] = 0x00; sensor_data[1] = 0x00; /* Enable I2C1 acknowledgement if it is already disabled by other function */ I2C_AcknowledgeConfig(I2C1, ENABLE); /* While the bus is busy */ while(I2C_GetFlagStatus(I2C1, I2C_FLAG_BUSY)); /*----- Transmission Phase -----*/ /* Send START condition */ I2C_GenerateSTART(I2C1, ENABLE); /* Test on EV5 and clear it */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT)); /* Send sensor address */ I2C_SendData(I2C1,0xF1); /* Test on EV6 and clear it */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_RECEIVER_MODE_SELECTED)); /* Read a byte from the sensor*/ sensor_data[0] = I2C_ReceiveData(I2C1); /* Test on EV7 and clear it */ while(I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_RECEIVED)); sensor_data[1] = I2C_ReceiveData(I2C1); /* Test on EV7 and clear it */ while(I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_RECEIVED)); /* Send I2C1 STOP Condition */ I2C_GenerateSTOP(I2C1, ENABLE); After i send out the address of the sensor, i'm seeing (on the scope) two byte of data with 18 clock cycles. I assumed this data is only read out using I2C_ReceiveData? Also is a NACK command required before stop commmand? Any suggestions about what I'm not doing correctly would be greatly appreciated. -- Thanks #embedded-c