Skip to main content
ANaga.2
Associate III
January 18, 2021
Question

Quectel M66 with STM32L476RG

  • January 18, 2021
  • 0 replies
  • 676 views

Hi,

Hope everybody is doing great !

I am trying to have quectel M66 2G modem running along with our application running on L476RG.

I found the celluar package from ST for B96 modem and could integrate it to our application and it has all the features we need for our project.

I could get it work with M66 upto sim init. but when I try to register to a network with valid apn details, the ATcommand AT+QICSGP is throwning error. I understood that this AT command does different thing for BG96, I tried AT+QIREGAPP for M66, even this is giving error.

Could anyone please give me hints on this.

Best Regards,

Ankush Nagaraju

This topic has been closed for replies.