Skip to main content
prsh
Associate III
November 2, 2022
Question

Quad-SPI with STM32H7

  • November 2, 2022
  • 0 replies
  • 546 views

Hello , wanted to interface QSPI dual flash with STM32H743Zit6 . The External Flash memory i am using is sst26vf064b . I am having 2 of this Flash memory on my hardware Can anyone help me with the same?

I am trying to read the ID data

First -- With SPI

sCommand.InstructionMode  = QSPI_INSTRUCTION_1_LINE;

sCommand.Instruction   = 0x9F;

sCommand.AddressMode = QSPI_ADDRESS_NONE;

sCommand.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;

sCommand.DataMode = QSPI_DATA_1_LINE;

sCommand.DummyCycles   = 0;

sCommand.Address    = 0;

sCommand.DdrMode    = QSPI_DDR_MODE_DISABLE;

sCommand.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;

sCommand.NbData = 3;

 HAL_QSPI_Command(&hqspi, &sCommand, 1000);

 HAL_QSPI_Receive(&hqspi, ID_REG, 1000);

it is giving me {0x01,0x20,0x18} as output which is not the expected output

Second -- with QuadSPI,

Enable QuadIO

sCommand.InstructionMode = QSPI_INSTRUCTION_1_LINE;

sCommand.Instruction = 0x38;//READ_CONFIGURATION_REG_CMD;

sCommand.AddressMode = QSPI_ADDRESS_NONE;

sCommand.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;

sCommand.DataMode = QSPI_DATA_NONE;

sCommand.DummyCycles = 0;

sCommand.DdrMode = QSPI_DDR_MODE_DISABLE;

sCommand.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;

sCommand.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;

sCommand.NbData = 0;

HAL_QSPI_Command(&hqspi, &sCommand,1000);

sCommand.InstructionMode = QSPI_INSTRUCTION_4_LINES;

sCommand.Instruction = 0xAF;

sCommand.AddressMode = QSPI_ADDRESS_NONE;

sCommand.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;

sCommand.DataMode = QSPI_DATA_4_LINES;

sCommand.DummyCycles = 2;

sCommand.DdrMode = QSPI_DDR_MODE_DISABLE;

sCommand.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;

sCommand.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;

sCommand.NbData = 3;

HAL_QSPI_Command(&hqspi, &sCommand.1000);

HAL_QSPI_Receive(&hqspi, &ID_REG[0],1000);

which gives me output as {0x88,0x88,0x88}

This topic has been closed for replies.