Question
Problems with Keil and F3 discovery
Posted on December 04, 2012 at 13:08
Has anyone else got the F3 discovery working with Keil uVision? The code compiles but when starting a debug session it doesn't seem to deploy and it displays all zeros for the code on the device.
I'm using the latest uVision 4.6 and happily connecting to my F4 discovery so don't think I've made a basic mistake. (Not tried a F0 discovery yet but I will.) I checked the guides and believe everything is set up correctly.STLink is showing up as expected as a USB device in Win7 and is identified in the debug tab for the project properties. The board is powered up and happily running the demo code.Any tips? Anyone happily coding away?