Skip to main content
z__it
Associate
January 22, 2016
Question

Problem with Readout Protection on STM32F4 Discovery

  • January 22, 2016
  • 3 replies
  • 734 views
Posted on January 22, 2016 at 07:43

I cant connect my board because of readout protection is activated (Level 1) and I cant set it back to level 0 in Option Bytes menu on ST-Link Utility. How can I disable Readout Protection  please explain in an easy way.

thank you
    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    January 22, 2016
    Posted on January 22, 2016 at 14:50

    Did you enable the readout protection? Or are you just having connectivity issues?

    Try strapping BOOT[0] to VDD

    Alternatively you could use the System Loader to walk the part out via the USART, I believe I've covered the technique here before.

    The easy way is to provide a method in your own code to undo the protection. ie you code a method in and out

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
    z__it
    z__itAuthor
    Associate
    January 23, 2016
    Posted on January 23, 2016 at 09:59

    it's automatic level up to 1 and i dont know why.

    i tried connect Boot0 to Vdd and Boot1 to GND, USART was connected, and used flash loader demon before but it wasn't work. it cant connect to the board. 

    Tesla DeLorean
    Guru
    January 23, 2016
    Posted on January 23, 2016 at 18:46

    Ok, lets start with the basics. Make sure you are using a good USB cable, and that you have current versions of the drivers, ST-LINK Utilities, and firmware on the ST-LINK

    Try connectivity on a different USB port, a different PC, a different cable

    What version of Windows are you using here.

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..