Skip to main content
lukasz239955_stm1_stmicro
Visitor II
November 27, 2015
Question

problem with programing aplication

  • November 27, 2015
  • 2 replies
  • 555 views
Posted on November 27, 2015 at 09:26

Hi all,

I have a problem with programing STM32L15V.

I am using about 1m long connection to device from ST Link V2.

When I am using STM32 ST-LINK Utility (V3.7.0) there is no problem with connection/programing/erase.

When I try to use ST-LINK_CLI (V2.3.0) from command line I can not connect to microcontroler.

I have need to use CLI as I need to automate process using LabView.

Any idea ?

Br,

Lucas
    This topic has been closed for replies.

    2 replies

    Nesrine M_O
    Associate
    November 30, 2015
    Posted on November 30, 2015 at 12:43

    Hi Lucas,

    “When I try to use ST-LINK_CLI (V2.3.0) from command line I can not connect to microcontroler.�

    You may ignored some parameters in your connect command, so it uses the default ones

    try this -c SWD UR

    -Syrine-

    shahril rizal hassan
    Associate
    October 12, 2017
    Posted on October 12, 2017 at 03:56

    Hi Lucas,

    I working to automated the CLI process using labview also...can you share the labview vi to me?

    Best regards,

    Shahril