Skip to main content
adeemkazi92
Associate III
October 16, 2015
Question

problem with 7 segment on stm32

  • October 16, 2015
  • 0 replies
  • 418 views
Posted on October 16, 2015 at 09:36

i am workin on diplaying no''s on 7 segment via stm32f072b

the problem is that the o/p is not appearing on the 7 segment

ive connected pins of 7 seg to gpioA and gpioC via a 3.3k resistor

the follwing is the code

#include ''main.h''

//------------------------------------------------------------------------------

// Function Name : Init _GPIO pins

// Description : pins ,port clock & mode initialization.

//------------------------------------------------------------------------------

void Init_GPIO(void)

{

/* GPIO config */

GPIO_InitTypeDef GPIO_InitStructure;

/* GPIOA GPIOB clock enable */

RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA | RCC_AHBPeriph_GPIOC, ENABLE);

/* Configure 8 ,9 PINS as input floating */

GPIO_InitStructure.GPIO_Pin =GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 ;

/* Configure PORT clock speed */

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_10MHz;

/* Configure PORT mode as input */

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;

/*configure PINS to output pushpull mode*/

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

/* Above all GPIO instructions apply to port ''C''*/

GPIO_Init(GPIOC, &GPIO_InitStructure);

/* Configure 8,9,10,11,12,13 pins as input floating */

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 ;

;

/* Configure PORT clock speed */

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_10MHz;

/* Configure PORT mode as input */

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;

/*configure PINS to output pushpull mode*/

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

/* Above all GPIO instructions apply to port ''B''*/

GPIO_Init(GPIOA, &GPIO_InitStructure);

}

/*******************************************************************************

* Function Name : main

* Description : Main program.

*******************************************************************************/

int main(void)

{

Init_GPIO(); //calling a function

while(1)//infinite loop

{

/*ODR bits can be individually set and reset */

//for displaying 0

GPIOA->ODR = 0x0007;

GPIOC->ODR = 0x0007;

}

}
    This topic has been closed for replies.