Question
Problem while I load build output to STM32F411 through ST-LINKV2-1 or V2
Posted on June 26, 2015 at 11:14
Dear
I tried to upload build output(.axf) into flash of STM32F411, but it failed.- Internal command error - Error: Flash Download failed - Target DLL has been cancelled.I used STM32F411 Nucleo board pulled out two jumpers for ST-link not Nucleo. Target board is my own board before it succeed on loading. The target board is consists of STM32F411. I started to develop from Nucleo, then moved to target board.Loading .axf process is succeed on Nucleo, but when I used it as ST-link with the other target board it failed.Wiring is same as before.Is there any suspicious things?Regards,Jiwon #st-link-stm32f411