Skip to main content
sabasit2006
Associate II
October 31, 2008
Question

Peripherals interfacing

  • October 31, 2008
  • 2 replies
  • 528 views
Posted on October 31, 2008 at 06:33

Peripherals interfacing

    This topic has been closed for replies.

    2 replies

    brianforde9
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:50

    The signal interfaceing should be straight forward. Address - Address, and Data - Data, nOE, nWE, etc.

    As regards the address map, it is quite simple really. Depending on which chip select line you use for your peripheral (FSMC_NE1 / FSMC_NE2 / FSMC_NE3 / FSMC_NE4), it will be accessable at 0x60000000, 0x64000000, 0x68000000, or 0x6C000000. Your device will appear in Bank 1 (NOR/PSRAM).

    You must set up the FSMC timings as appropriate to your peripheral.

    Refer to

    http://www.st.com/stonline/products/literature/rm/13902.pdf

    , Section 18.4, for further detail.

    sabasit2006
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:50

    Dear,

    I am using STM32F microcontroller. I have a query related peripherals interfacing with MCU.

    Question:

    How do I interface 8-bit peripheral chips like MT8980 (Digital Crosspoint Switch), M34116 (PCM Conference Chip), etc with the STM32F103ZET6 MCU?

    In the memory mapping diagram, there are FSMC banks used for memory mapping. Kindly tell me what should I do for the I/O mapping at which address locations?

    reply as soon as possible.

    regards,

    S.A.Basit